Wire winding is a crucial step in motor manufacturing that directly affects motor performance, so winding machines require higher standards of speed and precision than other machines.

The PC-Based Host Motion Controller AX-8 Series serves as the center of the control layer. Its modular CODESYS platform enables fast and stable motion control, achieving a highly flexible automatic process; the Human Machine Interface DOP-100 Series provides user-friendly interfaces for visualized operation, allowing users to create and modify the winding sequence efficiently.

The solution employs the AC Servo Drive & Motor ASDA-B3 Series for precise, synchronous motion control to execute stable and high-speed winding.