Delta’s 4-head Labeling Machine Solution is widely applied in beverages, industry, pharmaceuticals, dietary supplements, and more.

The labeling process starts with bottle conveying. The bottle spacing axis separates and then the calibration axis straightens bottles. When the sensor detects a bottle is approaching, the label roll is stretched and unwound by the feeder for precise feeding and fast labeling. Finally, the conveyor belt sends the bottles away to complete the label processing.

The conveyor belt, bottle spacing axis, and calibration axis in Delta’s 4-head Labeling Solution adopt Sensorless Vector Control Compact Drive VFD-EL-W Series. Moreover, the 4-head label feeding axis is equipped with the Standard AC Servo System ASDA-B3 Series to conduct precise, smooth motion control for high production efficiency and capacity.

The control layer adopts the PLC-Based Motion Controller AX-3 Series and Modbus communication to transmit data to the intuitive and user-friendly Human Machine Interface DOP-100 Series, connecting operators and equipment together for more efficient management.