Delta is participating in TIMTOS 2023 from 3/6 to 3/11 with the theme of “Cloud & On-Premises Integration for Sustainable Smart Manufacturing” to demonstrate exhibits including: “Manufacturing Operation Visualization”, “CNC Industry-Specific Applications”, “Smart Manufacturing Integration”, “ESG Fulfillment for the Industry”, and “Smart Machines”.

Delta demonstrates its newly upgraded CNC controller NC5 Series with newly built-in industry CAD/CAM which can automatically identify graphics, generate G Code with one click, and support tool path simulation to shorten production and enhance productivity.

Delta exhibits its CNC lathe machine, milling machine, woodworking router, multi-spindle machinery solutions with the CNC controller NC5 Series. The CNC IIoT architecture of the solutions helps manufacturers optimize management efficiency and shape the future of smart machining.

Delta showcases the Smart Screwdriving Solutions for Assembly, providing handheld and integrated robotic arm solutions with the Smart Screwdriving System to complete metal production from machining to assembly.

Delta demonstrates the 5-axis machining center at TIMTOS 2023. The CNC controller NC5 Series is the solution core integrated with the Module Robot RS-M90E7, which combines the advantages of industrial and collaborative robots to showcase the future direction for machine tool transformation.